Motion Control Products

Wide Variety of Motion Control Solutions

Same Day Shipping - Over 1,200 products available to ship same day.

Committed to Professional Support - Online, on the phone and in-person.

Global Sales and Support

2-Year Warranty

Support & Information

Free Shipping Offer*

With over 1,200 of our most popular products available for same day shipping (up to 10 pieces) and thousands more available within 7 business days, Oriental Motor can easily meet your delivery needs. Now Oriental Motor is offering FREE UPS Ground shipping for all online orders.*

*Terms & conditions apply.

Technical Support
Technical Support

1-800-GO-VEXTA
(468-3982)

Operator Manuals

To download an operator manual please click the link below and search for the product you require. If you are unable to locate a particular opertor manual or have questions regarding the availability of certain manuals please contact Technical Support at 1-800-GO-VEXTA (468-3982).

Click here to search for an Operator Manual.

Product Lead Time

Product Lead Time can be found in the Online Product Catalog listed under Specifications as "Available to Ship". For lead time on quantities larger than 10 pieces please contact your local sales office.

For products available to ship same day, orders must be received no later than 12pm PST.

RoHS Compliant Products
RoHS

Oriental Motor offers RoHS versions of all of our most popular product lines. To learn more about RoHS and the products we offer contact your local sales office or visit our RoHS section.

All RoHS compliant products available online have the RoHS mark. In addition you may use the RoHS complaint product choice in the Search Products section.

Safety Standards

The following marks are indicated on the nameplates of approved products. Learn More.

ULUL recognized component.

ULRecognized to Canadian safety requirements under the component Recognition Program of Underwriters Laboratories Inc.

ULRecognized to Canadian Safety requirements and UL under the component Recognition Program of Underwriters Laboratories Inc.

CSACSA certified component.


ENEN and IEC certified component (indicates that VDE, TÜV Rheinland or DEMKO has certified that the product meets EN or IEC standards.)


CECertified CE marking for compliance with EC Directives (safety).

JETJapanese Safety Standards for Electrical Equipment Certified by Japan Electrical Safety & Environment Technology Laboratories.

CCCChina Compulsory Certification safety license for selling or exporting to China.

Technical Seminars

Responding to customer requests for in-depth training, Oriental Motor offers Free Motion Control and Technical Seminars. Targeted towards the needs of local industries, Motion Fair included technical seminars, one-on-one engineering assistance and product displays. Motion Fair is a technical training and information-sharing event for customers and partners of Oriental Motor. Motion Fairs are held throughout the year at various location in the United States.

For more information on the next Motion Fair in your area register for the FREE technical seminars and an Oriental Motor representative will contact you with the details.

Customer Feedback

Customer Satisfaction is more than a tagline for Oriental Motor it is our mission. We are continuously improving our online resources to provide you with the best internet experience possible. Let us know how we're doing. Oriental Motor is committed to total customer satisfaction. Click here to send us your feedback.

 

FAQ
Search FAQ GO
Category
  • Stepping Motor Systems
  • EMP Series Programmable Controller
  • AlphaStep Closed Loop Step Motor System
  • RK Series 5-Phase Microstepping System
  • AC Motors & Gearmotors
  • Electromagnetic Brake Motors
  • SB50 Brake Pack
  • Cooling Fans
  • General
  • Gearheads
  • Linear and Rotary Actuators
  • DG Series Hollow Rotary Actuators
  • EZ Limo Linear Actuators
  • DRL Series
  • Speed Control Systems
  • BX Series Brushless DC Speed Control
  • Brushless DC Speed Control Systems
  • BHF Series AC Speed Control
  • AXH Series Brushless DC Speed Control
  • ES Series AC Speed Control
  • Safety Standards
  • Website
  • Questions
    1. When ordering an extension cable, will it come with both the motor/driver cable and the encoder/driver cable?
    2. What is the accuracy of the BX in positioning mode?
    3. What is the backlash of the GFH-type gearheads used with the BX?
    4. Does the BX have dynamic braking capability? Can I stop the motor instantaneously without external component?
    5. Can we scale the OPX1A to display the gearhead speed rather than the motor shaft speed?
    6. Can we change speeds on the fly?
    7. If I have more than one BX series do I need an OPX-1A for each system or can I use one to program them all?


    Questions & Answers
    When ordering an extension cable, will it come with both the motor/driver cable and the encoder/driver cable?
    Yes, it will come with both. Only one part number is needed for both cables, which are necessary for proper operation. There are 2 options, however, the standard version and the flexible version.

     
    What is the accuracy of the BX in positioning mode?
    +/- 0.72°, which is determined by the encoder’s resolution.

     
    What is the backlash of the GFH-type gearheads used with the BX?
    1-2°, which is similar to our GN, GU, & SH gearheads.

     
    Does the BX have dynamic braking capability? Can I stop the motor instantaneously without external component?
    Yes. When the BRAKE input is Off, the dynamic brake takes effect, and the motor comes to a quick stop. Otherwise, the motor will decelerate to a stop when using START/STOP signal.In all cases, there is no holding torque unless a magnetic brake is supplied.

     
    Can we scale the OPX1A to display the gearhead speed rather than the motor shaft speed?
    Yes. This can be changed to up to 1000 (by increments of 1). The default value is 1. See the manual under Control Parameter, Speed Reduction Ratio.

     
    Can we change speeds on the fly?
    Yes, in speed control mode, you can change from 1 data set to another, thus changing the speeds on-the-fly. As long as the CW or CCW switch is ON, the binary code value of M0, M1, and M2 will determine the motor speed. The change in speed will occur at the acceleration (analog or digital) rate set.

     
    If I have more than one BX series do I need an OPX-1A for each system or can I use one to program them all?
    You do not need to buy an OPX-1A controller for each system. You can program one unit, disconnect it and program the others.