| |
 |
Before Using an AC Motor or
Gearmotor
|
 |
| |
 |
| Connecting
Gearheads to Motors |
 |
 |
As the figure to the right shows, a gearhead
is combined with a motor using the pilots
on each unit as guides. The gearhead should
be moved gently from side to side without
forcing the pinion shaft against the plate
of the gearhead (metal plate) or against the
gear itself.
Note:
Attempting to put a motor and gearhead together
by force may result in damage to the gearhead. |


| Mounting
GN Type and 5GU‚KA Type Gearheads |
 |
Mounting
5GU‚KHA Type Gearheads |
Use
the screws provided with the gearhead and
secure all the parts so that there are no
gaps between the motor flange face and the
pilot end face of the gearhead.
|
Before
mounting to machinery, assemble the motor
and gearhead using the screws provided with
the gearhead. Screws for mounting to machinery
are not provided. M8 screws must be provided
separately.

|
|
|
| Mounting
FPW Series, V Series, BH Series and BHF Series
Parallel Shaft type Gearheads |
Mounting
Right-Angle Gearheads |
The
V Series, BH Series and BHF Series parallel
shaft gearmotors come with the motor and its
dedicated gearhead pre-assembled. Mount to
machinery using the "mounting screws"
provided. FPW Series should also be mounted
using the stainless steel mounting screws
provided.

|
Attach
the provided gasket between the motor flange
face and the pilot end face. Do not bend or
scratch the gasket. Before mounting the right-angle
gearhead to the machinery, assemble the motor
and the gearhead using the screws provided.
(BH Series and BHF Series right-angle come
pre-assembled with the motor and its dedicated
gearhead.) Screws for mounting to machinery
are not provided. M6 screws (for GN type)
or M8 (for GU type, BH Series and BHF Series
right-angle) must be provided separately.

|
|
|
| Mounting
a Decimal Gearhead to GN Type and 5GU‚KA
Type |
Dimensions
for Mounting Holes |
Use
the screws provided with the decimal gearhead
and secure all the parts so that there are
no gaps between the motor flange face and
the pilot end face of the decimal gearhead,
or between the decimal gearhead and the gearhead's
pilot end face.

|
The
dimension of the 4 motor mounting holes are
shown as the pitch diameter in the dimensions
of each product. The distance between the
mounting holes are shown below.
 |
Unit
= inch (mm)
Motor
Frame Size |
A |
B |
C |
‚1.65
(‚42) |
1.89
(48) |
1.336
(33.94) |
1.4803
(37.6) |
‚2.36
(‚60) |
2.76
(70) |
1.949
(49.50) |
2.1260
(54) |
‚2.76
(‚70) |
3.23
(82) |
2.283
(57.98) |
2.5197
(64) |
‚3.15
(‚80) |
3.70
(94) |
2.617
(66.47) |
2.8740
(73) |
‚3.54
(‚90) |
4.09
(104) |
2.895
(73.54) |
3.2677
(83) |
‚4.09
(‚104) |
4.72
(120) |
3.341
(84.85) |
3.7008
(94) |
|
|
| |
|

Mounting
Method for Hollow Shaft Type Gearheads
Example of Attaching the Load |
Attach the load according to load shaft conditions
as shown in the
figure below. The hollow shaft inside dimension
is machined to a tolerance of H8, and incorporates
a key slot for load shaft attachment. A load
shaft tolerance of h7 is recommended. The key
provided with the product should be secured
to the shaft. Also, apply a lubricant such as
molybdenum disulphide grease to the load shaft
and the inner circumference of the hollow shaft.
The recommended dimensions of the load shaft
are shown in the table to the right. |
 |
 |
| 4GN‚RH,
5GN‚RH, 5GU‚RH |
 |
BH
Series, BHF Series Right-Angle Hollow
Shaft Type |
| Stepped-down
shafts
Straight
load shafts
|
|
Stepped-down
shafts
Straight
load shafts
|
| |
|
| |
|
|

Method of Securing the
Load to an Output Shaft
|
The
output shafts of high-power gearheads
are provided with a key slot to secure
the load, while the shafts of gearheads
with comparatively low power have been
given a shaft flat. Round shaft motors
come in two types, those with and without
a shaft flat on the motor output shaft.
|
 |
Shaft
Flat
0GN,
2GN, 3GN, 4GN, 5GN, 4GN‚RAA,
5GN‚RAA gearhead AXH015
and round shaft type motors with
a motor frame size of 3.15 inch
(80mm) or larger.
|
 |
 |
| |
|
 |
Key
Slot
5GU, 5GC, 5GCH, 5GU‚RAA, RH
Gearheads, 5GU‚KHA, V Series,
BH Series,FBL II Series, AXH Series
(except 15 W) |
 |
|
 |
On round shaft types, the output shaft
is machined to the accuracy of H7 in dimension
and 0.0008 inch or less in eccentricity.
Therefore, when connecting a load to the
shaft if the device, take measurements
using a dial gauge or similar instrument
so that there is no eccentricity. When
the shaft center of two shafts does not
fit, use a flexible coupling (MCL coupling)
etc. to avoid unnecessary strain on the
shaft. The same procedure should be applied
when securing a load to gearheads. |
|
Securing
the Load to a Shaft Flat
With
a shaft flat, use a locking screw
to ensure that the lead does not
slip. We recommend using double
point screws or other screws with
strong locking power.
|
 |
 |
| |
|
 |
Securing
the Load Using a Key Slot
Secure loads using the key provided
with the gearhead after machining
the key slot on the equipment
to be connected (sprocket etc.).
Note:
Ensure that the gearhead shaft
is not subjected to shock in the
axial direction, since this will
have an adverse effect on the
bearings. Be especially careful
not to use a hammer when inserting
the key. |
|
 |
|
| |
|
|
| |
|
|
|
| |
|
 |
|
| |
|
|
|