In order to realize various types of motion according to the needs of the times across the broad range of industries, such as medical care, food and transport, Oriental Motor has developed and delivered the optimal products around the world.
There are so many engineers all over the world who tirelessly exert themselves to develop new products and equipment while making improvements on their existing ones. Such engineers may face challenging moments from time to time, wishing that they would be able to create a certain type of motion with a specific control that would make it possible for them to meet a particular need. Oriental Motor has been helping these engineers accomplish their goals through a variety of products and services, and this has been our unwavering approach to business for decades.
We promise our customers that Oriental Motor’s first product will lead them to take the first step toward reaching their full potential for creativity.

To build a society where people can live a secure and sustainable lifestyle pleasantly through the things we have built together with our customers — both tangible things such as products and intangible things such as systems, technologies and user experiences.
To provide support through our motion control systems - via hardware, software and human aspect - for engineers (i.e. our customers) who strive taking thefirst step to make our tomorrow better.Providing our motion control systems to such engineers enables us to deliver experiences and excitements that not only meet but also surpass their expectations, while allowing us to create value that provides the "Wow!" factor around the world.
At Oriental Motor, we share our action guidelines (values) throughout the company and pursue the realization of our mission and vision.
Oriental Motor began with handmade motors in 1885 and we aim to carry on working on all kinds of "Motion" in the world, such as AC Motors, Speed Control, Position Control, Mechanical Motion and Thermal Management requirements. Oriental Motor globally has been providing the optimal motion systems as part of our total service, to meet the widest market demands.
Oriental Motor's sales and service network is international, with offices throughout North America, Europe and Asia.
We are following through on our basic stance of "being able to not just deliver a hundred units to one company but deliver one unit to a hundred customers" by standardizing products. This philosophy allows us to deliver what is needed, when it is needed, in just the quantity that is needed. This approach has also taught us what kinds of motion is required in every era such as high efficiency motors to meet the demands for more energy saving, lower heat generation and more precise motion required in today's environment. We communicate with our customers from the stage where they start studying their equipment through the delivery and after sales service. This is the character of total service and support offered by Oriental Motor.

Oriental Motor's lead time is characterized by best in class (please contact us for specific products and quantities). Your order is shipped using only reputable carriers or any carrier of your choice to ensure the on-time and damage free-delivery.
Our manufacturing processes support our quick delivery and short lead times to allow us to support your needs. Our Just-In-Time production system allows the manufacturing of an order with little notice, in any quantity requested. Additionally, our one-by-one process allows us to manufacture one product as easily as one hundred.
Products and technology are only valuable when coupled with skilled people and services to support them. ORIENTAL MOTOR U.S.A. CORP. has dedicated over 25 years to establishing a service and support system to better serve customers. It is our goal to provide the best product and service from the design phase, through the sale and beyond. Please call on us to meet your motion control needs.
Since our success in standardizing compact motors, we have been developing products to match all kinds of motion. Copiers in the 60s, personal computers in the 70s, ATMs in the 80s, semiconductor manufacturing equipment in the 90s, and digitalization and environmentalism in recent years. We will keep on creating motion to meet society's needs in the future.


Oriental Motor offers a full line of Stepper Motors, Servo Motors, AC Constant Speed and Speed Control Motors, Brushless DC Motors, Linear and Rotary Actuators, Industrial Robots and a full line of Cooling Fans.
Oriental Motor's αSTEP closed loop control systems perform accurate positioning operations with ease. The αSTEP features a unique control system combining the benefits of "open loop control" and "closed loop control".
With the αSTEP control system, the position of the motor is always monitored and then the driver automatically switches between the two types of control depending on the situation. Under normal circumstances the operation of the motor is monitored and control is applied using open loop like a standard stepper motor. If an error occurs between the command and motor position due to a load or the like, the system immediately switches to closed loop control like a servo motor. This corrects the position and speed maintaining the desired operation. The combination of these two control methods ensures high reliability and performance.
A stepper motor is used to achieve precise positioning via digital control. The motor operates by accurately synchronizing with the pulse signal output from the controller to the driver. Stepper motors, with their ability to produce high torque at a low speed while minimizing vibration, are ideal for applications requiring quick positioning over a short distance.
Oriental Motor offers two types of servo solutions. Tuning Free Servos products or Short Range Servo products. Both types of solutions provide closed loop control along with many other advantages.
Our Tuning Free Servos are traditional servo solutions where the encoder provides feedback to the driver and all motion is controlled through a Position Counter. Use of the limited duty region is available for short periods of time where more torque is required.
Our Short Range Servos are closed loop as well and utilize a different motor technology where as they provide maximum torque throughout their entire speed torque range without the concern of operating in the limited duty region. See the speed torque comparison below for a clear comparison. Also, our Short Range Servo driver are Network compatible.
Motors offer excellent controllability and are therefore used as the drive sources of various automated equipment. In many cases a motor is combines with various mechanical components such as a ball screw, belt and pulley, and rack and pinion to convert the motor rotation to a different type of motion needed to drive the equipment. Oriental Motor has various linear actuators consisting of a motor assembled with the necessary mechanical components to meet the various needs of automated equipment.
The DGII Series is a line of of products that combine a high rigidity hollow rotary table with a closed loop stepper motor and driver package. It retains the ease of use of a stepper motor, while also allowing for highly accurate positioning of large inertia loads.
Brushless DC motors from Oriental Motor can achieve up to 970 lb-in of torque when combined with a standard geared option and with their space savings design contribute to a compact and powerful solution ranging from 15 W up to 400 W. With their flat torque, can produce rated torque from low to high speeds easily. Brushless DC motors also feature a wide variety of pre-assembled geared and electromechanical break options and are available with our industry leading stable lead times.
For applications where variable speeds are necessary, typically an AC motor with an Inverter or brush motors are used. Brushless DC motors are an advanced option due to their wide speed range, low heat and maintenance-free operation. Stepper Motors offer high torque and smooth low speed operation.
Speed is typically controlled by manual operation on the driver or by an external switch, or with an external 0~10 VDC. Speed control systems typically utilize gearheads to increase output torque. Gear types range from spur, worm or helical / hypoid depending on torque demands and budgets.
AC motors and gear motors include single-phase motors used with a single-phase AC power supply and three-phase motors used with a three-phase AC power supply. A single-phase motor can be operated by simply connecting it to a single-phase power supply via the supplied capacitor. A three-phase motor does not require a capacitor. All you need is to connect the motor directly to a three-phase AC power supply.
AC speed control motors and gear motors allow for the motor speed to be changed. By combining an AC motor with a dedicated control circuit speed changes can be performed. A broad lineup of AC motors & gear motors that can easily be used for speed control is available.
Oriental Motor offers a wide range of heat measure products centered on cooling fans to meet many diverse requirements. Our Axial Fans included large size and small sizes, long life versions and alarms. Our Centrifugal Blowers feature large static pressure and concentrated air flow. Our Cross Flow Fans feature a wide, uniform airflow and our Enclosure Fans are available in both suction and exhaust type.
Oriental Motor offers industrial network communication products under the FLEX concept, meaning each product is equipped with an interface that connects to various industrial networks and master controllers featuring I/O; such as PLC, HMI or serial communication such as RS-485 / Modbus (RTU).
FLEX is the generic name for products that are used for Factory Automation (FA) network control via I/O control, Modbus (RTU) control, or a network converter. FLEX products enable easy connection, easy control, and reduce the complexity of system configuration.
The OVR Series offers Articulated 4-axis, 5-axis, and 6-axis small horizontal transport robots, SCARA robots and Cartesian robots with a simple mechanism that can be easily controlled and constructed cost-effectively. Control with the MRC Series controller and AZ Series motor drivers.
Oriental Motor offers a wide range of motion control solutions that meet the needs of many various industries.
Oriental Motor products can also be found in a wide variety of other industries. With over 50,000 products to choose from, Oriental Motor can provide a product to meet the needs of most applications. From AC motors & gear motors, to stepper motor systems and controllers, to brushless DC motor speed control systems, to linear and rotary actuators and a full line of fans, no other motor manufacturer can provide a larger product breadth. Oriental Motor provides high quality, quick delivery and trained technical support.

From compact AC gear motors, to stepper motor systems, to a full line of fans. Oriental Motor products are widely used in the medical market. Applications such as raising and lowering a hospital bed or providing constant rotational speed in a centrifuge or ventilator require simple operation provided by AC gear motors. Stepper motors are used for precise positioning control in applications such as IV pumps, X-ray machines and blood analyzers. Applications such as an oxygen concentrator utilize fans for cooling. Compact size, high torque, low noise and reliability are just a few of the qualities that make Oriental Motor a perfect match to meet the requirements of most medical applications.

Oriental Motor's AC motors & gear motors and brushless speed control systems are widely used to meet automation needs throughout the packaging market. Products such as AC gear motors, including right angle and hollow shaft gearing options, are using in simple conveyor applications. IP67-rated watertight motors can be used in areas that need to be showered periodically. Clutch and brake motors are optimal for applications where simple index moves, such as labeling and cutting are required. Lifting applications often employ electromagnetic brake motors to provide braking in a power-off situation. For heavy industrial applications, Oriental Motor provides conduit and terminal box type motors, and for simple speed control we offer compact AC & brushless speed control systems.
Oriental Motor provides a wide variety of products to meet semiconductor equipment design needs. Our stepper motor systems address the torque, accuracy, resolution, smoothness and positioning required by applications such as pattern transfer, etching and dicing. AC motors & gear motors and brushless speed control systems provide compact size, flexibility, simple control, reliability and clean operation (no brushes). These products are perfect for applications requiring simple speed control and movement such as oxidation, photo-resist coating and wafer polishing.

Oriental Motor's wide product offering and Network products are widely used to meet many demands if Factory Automation (FA) applications. With our built-in controllers and network converters available to connect to many types of master controllers, PLCs and touch screens (HMI), our positioning motors, AC Speed Control motors, brushless motors, actuator products and thermo management products are designed for ease of use, simple installation and long life. There are many features built-in to each product that take the burden of programming off the master controller by incorporating programming or sensors for easy application design. Typical applications include Transport, grasping, pushing, pulling and cooling.

When a simple, small robot is the solution for automation. When automation needs to be implemented quickly. Oriental Motor is introducing the OVR Series of industrial robots to promote in-house production and advance automation.

As more and more companies seek to introduce machines to perform simple tasks, efforts to automate and save labor on
comparatively simple tasks such as moving goods, are ccelerating. One solution to this challenge has been the
introduction of transport robots (AGV/AMR/GTP).

New advancements in utilizing and protecting our environment include solar power generation, wind power generation, eco-cars and other technologies that contribute to energy saving and CO2 reduction, and other applications related to the development and manufacture of environment-friendly devices. Many of Oriental Motor's products are energy efficient and contribute to solving applications designed to reduce emissions and save energy over the life of the application.
Modern society requires diverse kinds of motion to make our lives easier. In the mechatronics field, technological innovation is constantly advancing, and the needs to be met by motors, such as drive sources, keep on diversifying. There is a need for motion that is faster and more precise, friendly to humans; for the environment, motion that is long-lasting as to do our bit in preserving the natural resources. In recent years, the range of our activities has broadened in fields related to environment friendly devices, such as eco-cars and solar energy generating systems.
We never stop developing diverse products for the times, ranging from AC Motors that run at constant speed to advanced motion, such as speed control and position control, and covering needs such as compliance with various field network standards, achievement of precise and rapid linear drive and adaptation to accurate Thermal Management. We offer a wide variety of around 50,000 products. We look at the perspective of our customers on the requirements of the motion, to deliver optimum drive systems.
Being the first motor manufacturer in Japan to offer standardized compact motors, Oriental Motor has continued its commitment to innovation and has expanded its field of technical expertise. We have created industry-standard motors for power and control applications used in both individual units and systems. Research and development of new products is conducted at all product plants in Japan, as well as the United States. With R&D on a global scale, Oriental Motor gains different perspectives into market expansion and customer requirements, resulting in the development of state-of-the-art technology to meet a wide range of needs. Our continuous research and development programs and tradition of quality guarantee that we meet the most rigorous specifications and deliver the highest standards of construction, ease of use and unequaled performance.
Our global Motion System covers research and development into motion, produces the right quantity of products for our customers whenever they need, with the service infrastructure to deliver products and information about motion whenever it is needed.
Business Hours:
Monday to Friday
8:30am EST to 5:00pm PST
Technical Support:
1-800-468-3982
Robot Support:
1-800-443-0775
Inside Sales Support:
1-800-448-6935
Customer Service:
1-800-418-7903