Improving the Quality of Printing Process Using Grip Conveyor

Issue: To Stabilize Grip Conveyor Speed and Improve Manufacturing Quality

Quality improvement is one of the most important issues in the factories of beverage manufacturers. Currently, two three-phase induction motors drive the grip conveyor, and printing while the bottles are clamped. Although an inverter is used for speed control, a speed difference occurs between the left and right belts, resulting in variations in the print position.

Challenge:

  • In the process of bottle printing using a grip conveyor (side conveyor), uneven belt speeds have caused printing positions to shift, resulting in inconsistent printing quality for each product.

Solution:

  • The Brushless Motor BMU Series Reduce Speed Variation to Stabilize Conveyor Speed and Improve Quality

The brushless motor BMU Series can stabilize the speed of the grip conveyor resulting in reduced speed difference and improved quality


The Brushless Motor With ±0.2 % Speed Regulation Maintain Constant Speed Even With Load Fluctuations

The brushless motor BMU Series always compare the set speed with the actual motor rotation speed. Since the voltage is adjusted as needed, the speed regulation (load) is ±0.2 %, enabling stable speed maintenance even when the load changes.

On the other hand, three-phase induction motors using conventional inverter control (V/f control) do not have a function to monitor actual rotation speed. Therefore, when a large load is applied, the rotation speed is greatly reduced. The speed regulation (load) is about -10 %, a significant difference compared to the brushless motor BMU Series.

Equipment such as grip conveyors, where the speed of the two motors must be precisely matched, would be well suited to use the brushless motor BMU Series.

Image of Using Three-phase Induction Motors (Label misalignment)

 

 

Image of Using the Brushless Motor BMU Series (No label misalignment)

 


 

[Comparison of Speed Variation (Reference values)]


Brushless Motors Contribute to Energy Savings

The brushless motor BMU Series are speed control motors that uses permanent magnets in the rotor, which is controlled by a circuit (driver). The energy-saving specification reduces power consumption and CO2 emissions. The 120 W output type of the brushless motor BMU Series reduces power consumption by approximately 26% compared to a 90 W three-phase induction motor, contributing to lower overall energy use for the equipment.


Flat and High-power Design Makes for More Compact Equipment

The brushless motor BMU Series are compact while also offering high power. With a 90 mm frame size, the overall length is 84.6 mm shorter than a three-phase induction motor with the same dimensions. Moreover, the output of the brushless motor BMU Series is 120 W, whereas the output of three-phase induction motor is 90 W, meaning output of the brushless motor BMU Series is about 1.3 times higher. Therefore, the brushless motor BMU Series will help reduce the overall size of the equipment.

Incidentally, the driver can be easily set to the desired rotation speed by turning the dial, and the rotation speed can be displayed, which is very popular among on-site workers.


Recommended Products

Brushless Motor BMU Series

Motor Rated Power

  • 30 W, 60 W, 120 W, 200 W, 300 W, 400 W

Gearhead Types

  • Parallel shaft gearhead
  • Right-angle gearhead
  • Hollow shaft flat gearhead



Engineering Notes
We're Here to Help

Service and Support

 

Business Hours:

Monday to Friday

8:30am EST to 5:00pm PST

 

Sales & Customer Service:

1-800-418-7903

Technical Support:

1-800-468-3982



©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved