Utilization Proposals of Motors in Accordance With Conservation Methods

Issue: Equipment downtime occurs or not sure when to replace equipment or if its cost or starting up with new equpiment will be extensive

Challenge:

  • Corrective maintenance is not appropriate for parts that have a major impact on equipment or facilities when they fail
  • Time-planned maintenance could be difficult if you don't know the replacement cycle of the parts, there will be a lot of waste.   Sometimes you have to replace a part even though it is still usable
  • Predicting maintenanec requires collecting and analyzing data for monitoring, initial investment in sensors and other equipment and ability to judge the analyzed data     

Solution:

  • Incorporate alarm functions to identify failures easily
  • Determine maintenance info like odometers and tripmeters for planned maintenance
  • Predict maintenance with constant monitoring to identify changes in accuracy or vairables like increased load on motor due to grease hardening over time

Do you have any of these concerns on site?

Corrective Maintenance

Equipment downtime has occured!
No action taken to deal with the situation

Preventive Maintenance

Time-Planned Maintenance Predictive Maintenance

Not sure when to replace

Isn't it hard to plan ahead?

Isn't it expensive to introduce equipment?

Equipment start-up seems difficult



 

About conservation methods

Flow chart map about conservation methods

Conservation Method

Advantages

Disadvantage

Corrective Maintenance

Simple and waste-free because it replaces failed parts.

This is not appropriate for parts that have a major impact on equipment or facilities when they fail.

Preventive Maintenance

Time-Planned Maintenance

Since parts are replaced according to a plan, you are unlikely to have unexpected problems.

If you don't know the replacement cycle of the parts, there will be a lot of waste. Sometimes you have to replace a part even though it is still usable.

Predictive Maintenance

Can help prevent problems before they occur. The parts to be replaced can be procured according to a plan without waste.

Since it is necessary to collect and analyze the data necessary for monitoring, initial investment in sensors and other equipment as well as skills to judge the analyzed data are required.



Oriental Motor’s extensive product lineup contributes to a variety of equipment maintenance.

Breakdown Maintenance - Products with Low Maintenance

AC Motor+Brake Pack (Alarm function)

Brake Pack SB50 W

[Applications] Running Multiple Conveyors
In order to detect abnormalities on the conveyor, sensors such as speed sensors and load cells must be installed.
In the case of the AC motor + brake pack, the alarm output from the thermal protector detection function allows visualization of stops due to conveyor locking, such as load stops.

 




Fan with Stall Alarm

DC Axial Flow Fan MD Series A Type

[Applications] When multiple fans are used for air agitation in a vegetable cultivation plant, etc. It is difficult to confirm fan failure by external appearance when the fan stops for an indeterminate cause.By outputting alarms from the fan, the failure location can be identified quickly.


Output Stall Alarm



Time-Planned Maintenance - Information Function Contributes to Planned Maintenance!

Odometer and Tripmeter Information to Manage Travel Distance

The time and amount of operation can be determined in advance based on a rule of thumb and the lifetime of the parts shown by the manufacturer, and maintenance can be performed according to a plan.

manage travel distance

Tripmeter Information
(INFO-TRIP)

This is output when the motor's travel distance exceeds the setting value.

Odometer Information
(INFO-ODO)

This is output when the motor's cumulative travel distance exceeds the setting value.

[Applicable Series]


Preventative Maintenance- Identifies Changes and Contributes to Timely Maintenance!

Constant Monitoring to Identify Changes in Status

Constantly monitors the condition of equipment and facilities, and performs maintenance when signs of "failure" are detected.

Case 1: Prevention by warm-up operation and grease-up

Identifies changes in increased load on the motor drive unit due to grease hardening over time. This will help you to prevent sudden equipment stops by taking measures such as warm-up operation and greasing up when the equipment starts.

Constant Monitoring to Identify Changes in Status

Case 2: Replacement at the end of product lifetime

When the ball screw drive is used for positioning operation, the sliding resistance changes from the initial high-accuracy state with pressurization to a lower value due to abrasion of the ball screw over time. By identifying the correlation between sliding resistance and positioning accuracy, it is possible to replace parts at the appropriate time.

At Equipment Start-up (Positioning accuracy: high)

State of high sliding resistance with applied pressure


When Used Up to Calculated Lifetime (Positioning accuracy: low)

The ball screw has been subject to abrasion and has low sliding resistance


 

Products that can constantly monitor the status of the load

αSTEP AZ Series Hybrid Step-Servo Product Family


Products that Support Maintenance

The following list introduces products and their functions that support maintenance.

Details of Each Series

Product Category

Series

AC Motors

Brake Pack SB50 W

Speed Control Motors

DSC

Brushless Motors

BMU

BLE2

BLE RS-485 Communication Type

BXII

BLV

BLH RS-485 Communication Type/Digital Setting Type

αSTEP

AR Built-In Controller Type

AZ Built-In Controller Type/
Pulse Input Type With RS-485 Communication

Stepper Motors

RKII

PKP/CVD RS-485 Communication Type Driver (2-Phase)

PKP/CVD RS-485 Communication Type Driver (5-Phase)

Cooling Fan

EMU

EMR

MRS

MRE

MD

MBD

MFD

 

Reduces Maintenance Load

The use of long life fans can reduce the number of times maintenance is required.
A long life fan capable of maximum 180,000 hours of continuous duty (approx. 20 years) is available.
The number of fan replacements is reduced, resulting in lower overall costs.

MRE Series Long Life Fans

AC Axial Flow Fan
MRE Series

MRE Series Long Life Fans

DC Axial Flow Fans
MD Series E Type

 

 


Engineering Notes
We're Here to Help

Service and Support

 

Business Hours:

Monday to Friday

8:30am EST to 5:00pm PST

 

Sales & Customer Service:

1-800-418-7903

Technical Support:

1-800-468-3982



©2026 - ORIENTAL MOTOR USA CORP. - All Rights Reserved